Programs

Programs are similar to program files in a
PLC-5
control application. Each program contains its own program-scoped tags (local data table), a main executable routine, and several optional subroutines.
Optionally, specify a fault routine for each program. The controller executes this routine if it encounters an instruction-execution fault within any of the routines in the associated program.
All controllers supported in the
Logix Designer
application <Version_Number> and later allow up to 100 programs per task.
The programs within a task execute from first to last.
When creating a project, the MainProgram is already defined for the MainTask.
Once a program is created, configure the main routine and then optionally configure the fault routine.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal