System Protocol no broadcasting

The selected protocol in the Controller Properties Dialog Box - System Protocol Tab Overview does not support broadcast messages. To send a broadcast message, the system protocol should be set to DF1 Master, DF1 Radio Modem, or DF1 Slave.
NOTE: Logix Designer versions 37 and later do not support controllers with serial ports. The
System Protocol
tab appears only in Logix Designer versions 36 and earlier for controllers with a serial port.
To configure the system protocol for broadcasting
  1. In the
    Controller Organizer
    , right-click the controller and choose
    Properties
    .
  2. Select the
    System Protocol
    tab.
  3. From the
    Protocol
    menu, choose
    DF1 Master
    ,
    DF1 Radio Modem
    , or
    DF1 Slave
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal