Program Properties Dialog Box - Configuration Tab Overview

Define program execution properties from the
Configuration
tab of the
Program Properties
dialog box.
TIP: To open the Program Properties dialog box:
  • From either the Controller Organizer or Logical Organizer, right-click the program to change and choose
    Properties
    .
Parameter
Description
Assign Main Routine
Select the Main routine assigned to this program from the pull-down menu.
Assign Fault Routine
Select the Fault routine assigned to this program from the pull-down menu.
Inhibit Program
Select the
Inhibit Program
check box if you want to prevent the controller from executing this program. The check box is cleared by default.
This check box is not shown if the
Use as Folder
check box is selected on the General tab.
Synchronize Redundancy Data after Execution
Select the
Synchronize Redundancy Data after Execution
check box to synchronize data at the end of the program execution.
TIP: The
Synchronize Redundancy Data after Execution
option only applies to standard controllers; it does not apply to Safety controllers.
This check box is not shown for non-Redundancy catalog numbers or if the
Use as Folder
check box is selected on the
General
tab. The check box is always enabled for controllers with Redundancy enabled as long as the controller is not in Hard Run mode. The check box appears dimmed when Redundancy is not enabled.
OK
Click this button to apply your edits and close the
Program Properties
dialog box.
Cancel
Click this button to cancel your edits and close the
Program Properties
dialog box.
Apply
Click this button to apply your edits and continue editing in the
Program Properties
dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal