Linear button

Select this button to change the selected cam segment to linear type. When all cam segments are linear, this button is disabled.
TIP: Selecting a cam point also selects the cam segment which follows it, so that both the cam point and cam segment are highlighted.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal