Go To dialog box

From the
Go To
dialog box, you can quickly navigate throughout the
Logix Designer
application. Depending on where you are in the system (for example, in the Language Editor, Data Monitor, or
Equipment Sequence
diagram editor), you can choose to:
  • Edit the base tag for the currently selected tag.
  • Display a cross reference for a tag.
  • Edit or monitor a tag.
  • Edit the properties of a tag or routine.
  • Set the row selection of the Tag Editor/Data Monitor on a tag.
  • Navigate to a specific location (for example, rung, line, grid location) in a routine.
  • Navigate to a called routine or a calling routine.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal