Force in Import/Export

If Force Masks are set in the project, they are exported. Upon Import, any Force Masks are input to the project, and the Online Bar indicator is set to Forces Installed.
The state of the Online Bar Forces Enabled indicator is not exported; upon Import, it is set to Forces Disabled.
An I/O Boolean operand with a variable index, such as Local:2:I.Data.[Index], where Index=0-15, cannot be forced in the ladder editor (all the Force menu items are all dimmed). However, if the operand bit index is absolute rather than variable, such as Local:2:I.Data.[0] or Local:2:I.Data.0, it can be forced.
TIP:
Editing force values in the export file is not recommended.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal