Transition firing states

The firing attribute is a subset of the FIRING state and gives a visual indication of the current state.
This firing attribute is visible when the transition expression has evaluated TRUE. The firing process requires several interactions with different phases and is an asynchronous process. Some phases may have programs that can take a long time to finish running (stopping a motor for example), so the firing object shows what the transition is doing. The displayed Firing Attribute values are: COMMITTED, STOPPING, RESETTING, PENDING, and PAUSED.
Firing Attribute
Description
ACQUIRING
The
Equipment Sequence
is acquiring the right to command the
Equipment Phase
. For every step that follows the transition, the
Equipment Sequence
must attach to each associated
Equipment Phase
before the steps can be activated.
COMMITTED
The transition is committed to firing because the transition expression has evaluated TRUE, but the transition cannot activate the following steps because it is in Manual mode or the
Equipment Sequence
is in the PAUSED substate.
STOPPING
As part of firing, the
Equipment Sequence
commands all the active preceding steps to stop. The transition firing state is STOPPING until all commanded steps are STOPPED.
RESETTING
As part of firing, the
Equipment Sequence
commands all the preceding steps that are STOPPED to RESET. The transition firing state is RESETTING until all the commanded steps are IDLE.
PENDING
The transition is not able to fire because the
Equipment Phase
s of the steps above or below the transition are not in the correct state to permit the transfer of control function.
PAUSED
The transition is committed to fire, but cannot because the
Equipment Sequence
has been PAUSED. The transition is waiting for a RESUME command.
POST SCANNING
The transition is at the end of the firing process. On the next scan of the
Equipment Sequence
chart, the transition advances the chart.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal