Change modes in an Equipment Sequence
Switch between
shows no highlighting, while the
shows light blue highlighting and a blue outline. Select to toggle between
Automatic
and Manual
mode in an Equipment Sequence
by
toggling the Change Mode
button. The Automatic
mode iconManual
mode icon Automatic
and Manual
mode.Before you begin:
- Go online with the controller.
- In the Sequence Editor, open anEquipment Sequence.
To change the mode in an
Equipment Sequence
:- SelectTake Ownership
to take ownership of the Equipment Sequence. - (optional) Start theEquipment Sequenceby selecting
. - Select
to go into Manualmode. - Once completing manually executing any steps or phases, select
to go back to Automaticmode.
Provide Feedback