Equipment Sequences

An Equipment Sequence is a series of Equipment Phases. The phases automatically run when the sequence is started, according to an order defined by the sequence. Use the
Logix Designer
application's Sequence Manager to create, edit, run, and monitor sequences.
Create an Equipment Sequence program to run a batch process within a Logix controller. A batch process combines raw materials, in a defined order, using one or more pieces of equipment to produce a fixed amount of product.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal