Delete button

Select this button to delete all selected cam element in the graph view, or to delete the selected lines in the grid view. A cam element includes a cam point and the segment immediately to the right of that point. For the output cam editor, a cam element includes the cam left and cam right positions, and the segment between them.
If no elements are selected, this button is disabled.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal