CST Timestamped Fuse Data

If a fuse is blown in an output-fused module, this option attaches a CST Timestamp to the Fuse Blown fault, indicating when the event occurred.
The timestamp reflects the time that the module detected the fault; if several faults occur in one message period, the timestamp reflects the time the last one was detected.
You can compare this timestamp with the current CST in the chassis containing the module in order to compute exactly when the fuse blew.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal