Advanced Project Documentation Configuration dialog box overview

Use the Advanced Project Documentation Configuration dialog box to configure the language localization that is downloaded to the controller.
Use the
Download Controller Description Language
parameter to switch the currently used documentation language, which changes the language used to display all project documentation.You can select languages that do not currently have content. The result is blank project documentation (if no default language is chosen) is displayed for the project.
The description of the controller is the only documentation downloaded to the controller. Only one translation of the description may exist in the controller at a time.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal