J

jerk rate
The maximum rate of change of the rate used to ramp output to input.
jog
To generate motion (continuous or incremental) whenever an operator-activated switch is closed.
joint axis
A rotary robotic coordinate axis typically having overtravel rather than rollover limits.
jump
A change in the normal sequence of program execution by executing an instruction that alters the program counter (sometimes called a branch). In ladder programs, a JUMP (JMP) instruction causes execution to jump to a labeled rung.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal