Run mode

Run mode
The controller mode during which logic is executing, inputs are read, the program is scanned, and the outputs are energized and de-energized. Editing operations are restricted. If the keyswitch is in Remote, the controller is in Remote Run mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal