Create and Configure I/O

In the
Logix Designer
application add all the I/O and Communication modules that are part of the project. This allows the controller to communicate with the modules.
When you configure an I/O module, you specify characteristics specific to that module. The
Logix Designer
application automatically adds the predefined tags for the module as controller-scoped tags.
The configuration information for the module depends on the module you select.
You can specify electronic keying to restrict a connection to a specific module type. Electronic keying ensures that a module being inserted or configured is the proper type.
Repeat this process for all of the modules your project works with.
To create and configure I/O
  1. In the
    Controller Organizer
    , expand the
    I/O Configuration
    folder, right-click a network or backplane and choose
    New Module
    .
  2. The
    Select Module Type
    dialog opens.
  3. Choose the module type to create:
    • Catalog - Choose from a list of modules that is valid for the current context
    • Module Discovery - Perform online module discovery to find attached physical devices on a network or backplane
    • Favorites - A custom list of module types
  4. After selecting the module, select
    OK
    .
  5. The
    New Module
    dialog box opens from which you can complete the process of creating and configuring the I/O module.
    Enter the configuration information for the module you are creating.
    • Name - Enter a name for the module, this name is appended to the catalog number in the
      Controller Organizer
      .
    • IP Address - For Ethernet connected modules, the IP address is required.
      For other settings, the default values are automatically applied.
  6. Select
    OK
    . The new module is displayed in the
    Controller Organizer
    .
    Double-click the module in the
    Controller Organizer
    to open it and review the default settings and edit them if needed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal