Program mode

Program mode
The controller mode during which logic is not executing, outputs are not controlled, and editing operations are available. If the keyswitch is in Remote, the controller is in Remote Program mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal