Wiring the OK Contacts

A set of isolated solid-state OK relay contacts is provided for optional interface to an E-stop string, which controls power to the associated drives. The OK contacts are rated to drive an external 24V pilot relay (for example, Allen Bradley 700-HA32Z24) whose contacts can be incorporated into the E-Stop string as shown below.
servo_OKcontacts
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal