When Interleave Interrupts is set Real Time Sample (RTS) period must be zero, Conversion Rate should be 1200 Hz and the Low Pass Time Constant should be none.

The Interleave Interrupts feature is not needed when the module is not configured for the fastest possible combination of RTS, Conversion Rate, and Low Pass Time Constant. Clear the Interleave Interrupts check box.
In order for the module to use this feature, you must set the:
  • Conversion Rate to 1200 Hz
  • Low Pass Time Constant to None
  • RTS to zero
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal