View Output Offset Results - FLEX I/O Calibration

To view the results of the offset calibration, perform the following step. You can see the results in the
offset
The steady-state deviation of a controlled variable from a fixed set point. In a linear function (y=mx+b), the parameter (b) is used to drive the dependent variable (y) to zero when the independent variable (x) is zero.
Status
column.
If the Status column displays:
Then:
OK
Select
Next
to perform the gain calibration.
Error
Select
Retry
to repeat the process.
You may also select:
  • Stop
    to cancel calibration and exit the calibration.
  • Help
    for assistance with this tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal