View Output Gain Results (FLEX I/O Calibration)

To view the results of the gain calibration:
gain
The ratio of the magnitude of the output signal with respect to that of the input signal.
In a linear equation (y=mx+b), the parameter (m) is used to drive the dependent variable (y) to a specified value when the independent variable (x) is at a maximum.
  1. Look at the
    Status
    column.
    IF:
    • OK
      appears, calibration is successfully complete.
    • Error appears, select
      Retry
      to retry to view the results of the gain calibration and notify you that calibration is complete.
  2. Select
    Finish
    .
    The software returns you to the
    Calibration
    tab.
You may also select
Help
for assistance with this tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal