View Input Gain Results - FLEX I/O Calibration

To view the results of the input channel gain calibration:
gain
The ratio of the magnitude of the output signal with respect to that of the input signal.
In a linear equation (y=mx+b), the parameter (m) is used to drive the dependent variable (y) to a specified value when the independent variable (x) is at a maximum.
Look at the
Status
column.
IF:
  • OK
    appears, select
    Next
    to perform gain calibration on the output channels.
  • Error appears, select
    Retry
    to repeat the process.
You may also select:
  • Stop
    to cancel calibration and exit the calibration.
  • Help
    for assistance with this tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal