User Program Value and Program State inconsistent

The User Program Value is non-zero, but the Program State is set to Hold Last State. The User Program Value must be zero if the Program State is Hold Last State.
Either set the User Program Value to zero, or set the Program State to User.
The User Program Value is a specific value set if the owner controller is switched into
controller
A device that controls machines or processes elements (for example, a programmable controller or relay panel).
Program mode.
Program mode
The controller mode during which logic is not executing, outputs are not controlled, and editing operations are available. If the keyswitch is in Remote, the controller is in Remote Program mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal