Time Base is out of range

This message appears when incomplete, incorrect, or conflicting configuration data are detected for Ch0StoredData2, when you entered a time base (in the Configuration Tag) that was not a multiple of 10, or when the time base is too large (>3000 ms, >3 sec).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal