Stopped Calibration

Clicking on the Stop button at some point during calibration leaves the module with a new offset coefficient and an old gain coefficient. The first line in this message varies, depending on where you are in the software.
The module is not calibrated. The module must be calibrated before it is used.
Click the Cancel button to continue the calibration with no effect from having pushed the Stop button. Clicking OK exits calibration, leaving the module in the uncalibrated state described in this message.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal