Signal exceeds range

The signal settings must be within the signal range for this module. Enter a signal within the range.
module
A device, typically an I/O device, that communicates with the controller. The controller, a particular 1756-IB16I or a PanelView are all considered modules.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal