Select PV Range Units

Use this dialog box to select units for the PV Upper and Lower Range values.
Parameters
Category
Select the category of the unit such as power, electrical, and temperature. Select "Enter ID Value" if there is no suitable category.
PV Range Units
Select the unit. This field appears dimmed if the category is "Enter ID Value".
PV Range Units ID
Displays the Unit ID associated with the unit.
OK
Click this button to accept your edits and close the dialog box.
Cancel
Click this button to close the dialog box without accepting your edits.
Help
Click this button for help on this tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal