Safe State should be zero if the output range is set to none

The output range is set to None, therefore, the Safe state value must be zero.
Change the Safe State value to zero.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal