Real Time Sample too large

The Real Time Sample (RTS) period is too large. Enter an RTS value that is 10,000 ms or less.
The RTS indicates how often the modules’ inputs are to be sampled and is entered in milliseconds. There is only one RTS for the entire module.
module
A device, typically an I/O device, that communicates with the controller. The controller, a particular 1756-IB16I or a PanelView are all considered modules.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal