Rate Alarm too large

The current Rate Alarm setting is too large. Select a smaller Rate Alarm setting from the Alarm Configuration Tab.
The Rate Alarm value indicates to trigger when the rate of change between input samples exceeds the setpoint. Set this alarm in terms of Engineering Units/Second.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal