Program Value outside Clamp Limits

The Program Value selected is outside the Clamp Limits. The Program Value must be within the programmed Low Clamp Limit and High Clamp Limit.
Either change the Low and/or High Clamp limits, or adjust the Program Value to be between the existing Clamp Limits.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal