Output Calibration Dialog Box - Gain Results Tab Overview (FLEX I/O Analog)
    The purpose of this tab is to:
- show you the results of the gain calibrationgainThe ratio of the magnitude of the output signal with respect to that of the input signal.In a linear equation (y=mx+b), the parameter (m) is used to drive the dependent variable (y) to a specified value when the independent variable (x) is at a maximum.
- notify you that calibration is complete
- give you the ability to return to the Calibration tab
You can see the results in the Status column.
| If the Status column displays: | Then: | 
| OK | Calibration is successfully complete. | 
| Error | Click Retry to retry to show the results of the gain calibration and notify you that calibration is complete. | 
     TIP: 
    
You must click the Finish button to return to the Calibration tab.
Provide Feedback