No Notch Filter value selected
    A current Notch Filter value has not been selected. It may have been changed to an invalid value in the Data Monitor or programmatically via Ladder Logic. Select a Notch Filter setting.
The Notch Filter attenuates the selected frequency and its harmonics in the input signal. Also, you can use the Notch Filter to filter out line noise.
Provide Feedback