Interleave Module Interrupts

A loss of data between the ControlNet Adapter and the module can occur for long periods of time under some system configurations. When enabled, this feature ensures exchange of time-critical data when channels are configured for the fastest update times. Do not check the Interleave Module Interrupts check box unless you know for certain that you have a specific use for this option. The Interleave Module Interrupts feature is useful only in limited circumstances and can only be enabled when you configure a module’s Conversion Rate to 1200 Hz, Low Pass Time Constant to None, and Real Time Sampling period to 0 for all channels on the module.
ControlNet network
An open control network that uses the producer/consumer model to combine the functionality of an I/O network and a peer-to-peer network, while providing high-speed performance for both functions.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal