High Alarm greater than High High Alarm

The High Alarm is greater than the High High Alarm. Enter a new High Alarm that is less than the High High Alarm.
  • The High Alarm is the level of input to a channel that will cause the module to trigger the High alarm. The alarm will remain until the input returns below this level, unless it is within the deadband, or as long as the alarm is latched.
    module
    A device, typically an I/O device, that communicates with the controller. The controller, a particular 1756-IB16I or a PanelView are all considered modules.
  • The High High Alarm is the level of input to a channel that will cause the module to set the High High alarm. The alarm will remain until the input returns below this level, unless it is within the deadband, or as long as the alarm is latched.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal