Fault Value and Fault State inconsistent

The Fault Value is non-zero, but the Fault State is set to Hold Last State. The Fault Value must be zero when the Fault State is Hold Last State.
Either set the Fault Value to zero, or set the Fault State to User.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal