Digital Filter too high

The Digital Filter time constant is too large. Enter a Digital Filter value that is less than 20,100 milliseconds.
The Digital Filter is a first order lag filter that smooths input transitions and is specified in milliseconds.
transition
The change of state from an Off to On condition or vice versa.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal