DANGER! A module identity mismatch has been detected - Please Read Carefully!

If you perform the selected operation you may interrupt control. You should choose to continue with the selected operation or cancel.
There is a mismatch between the actual module and what is specified on the General Tab. One or more of the following is different:
  • Vendor
  • Module Type (the combination of Product Type and Product Code for a particular Vendor)
  • Major Revision
While creating the module, you could have:
  • selected the wrong module
  • selected the wrong location
  • placed the wrong module in the location
Since the actual module is not what the software expects, the software may behave unexpectedly when performing the operation. An unintended part of the system may have its control interrupted.
Change the module configuration on the General Tab so that it matches the actual module.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal