DANGER! About to Reset Module - Please Read Carefully!
    This module is about to be reset which will break the connection to the module and re-configure it.
Control may be interrupted if you do this.
- Choose OK to continue with the reset operation.
- Choose Cancel to cancel the reset operation.
Provide Feedback