Calibration output values changed unexpectedly during the calibration process

The connection to the module must be inhibited while it is being calibrated. Cannot continue.
To continue with the calibration process, inhibit the connection to the module.
Access the
Connection
tab on the
Module Properties
dialog box to inhibit the connection to the module.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal