A CIP error occurred in the communications request

There was an unexpected Direct Communications messaging error. This could occur due to a module identity mismatch, or when the module does not accept the specified command.
Contact Technical Support for assistance.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal