View Network Communication Status

Network status information on the
Port Diagnostics
tab is displayed for informational purposes only, however you can select:
  • Refresh to query the module status information and display the current result.
  • Reset Counters to reset all network status elements to zero and begin counting again.
You must be online for these options to be available.
For more detailed information about the data displayed on this screen see
1756-ENET Port Diagnostics Tab Overview
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal