View Backplane Information, Status, and Chassis Information

The
Module Properties
dialog
Backplane
tab displays read-only information about the selected module. Additionally, select:
  • Clear Fault
    to remove the module’s backplane fault.
  • Refresh
    to display new data from the module.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal