Steps: To configure (Output State)

  1. In the
    Controller Organizer
    , right-click the module and select
    Properties
    .
  2. In the
    Module Propertie
    s dialog, select the
    Output State
    tab.
  3. Select the
    Channel
    button to select the channel to configure.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal