Record Low Calibration Values for Output Modules

The
Logix Designer
application commands the module to output specific levels of current. You must measure the actual level and record the results. This measurement allows the module to account for any inaccuracies.
To record low calibration values for output modules:
  1. Measure the output values using a multimeter.
  2. Enter the values in the appropriate
    Recorded Reference
    box.
  3. Select
    Next
    to proceed with calibration.
    • You may also select
      Stop
      to cancel the calibration.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal