PLC and SLC Error Codes (.ERR)

Logix firmware revision 10.x and later provides new error codes for errors that are associated with PLC and SLC™ message types (PCCC messages).
This change lets RSLogix 5000 software display a more meaningful description for many of the errors. Previously the software did not give a description for any of the errors associated with the 00F0 error code.
The change also makes the error codes more consistent with errors returned by other controllers, such as PLC-5® controllers.
The table shows the change in the error codes from R9.x and earlier to R10.x and later. As a result of the change, the .ERR member returns a unique value for each PCCC error. The .EXERR is no longer required for these errors.
PLC and SLC Error Codes (hex)
R9.x And Earlier
R10.x And Later
Description
.ERR
.EXERR
.ERR
.EXERR
0010
1000
Illegal command or format from local processor
0020
2000
Communication module not working
0030
3000
Remote node is missing, disconnected, or shut down
0040
4000
Processor connected but faulted (hardware)
0050
5000
Wrong station number
0060
6000
Requested function is not available
0070
7000
Processor is in Program mode
0080
8000
Compatibility file of processor does not exist
0090
9000
Remote node cannot buffer command
00B0
B000
Processor is downloading so it is not accessible
00F0
0001
F001
Processor incorrectly converted the address
00F0
0002
F002
Incomplete address
00F0
0003
F003
Incorrect address
00F0
0004
F004
Illegal address format - symbol not found
00F0
0005
F005
Illegal address format - symbol has 0 or greater than the maximum number of characters supported by the device
00F0
0006
F006
Address file does not exist in target processor
00F0
0007
F007
Destination file is too small for the number of words requested
00F0
0008
F008
Cannot complete request
Situation changed during multipacket operation
00F0
0009
F009
Data or file is too large
Memory unavailable
00F0
000A
F00A
Target processor cannot put requested information in packets
00F0
000B
F00B
Privilege error; access denied
00F0
000C
F00C
Requested function is not available
00F0
000D
F00D
Request is redundant
00F0
000E
F00E
Command cannot be executed
00F0
000F
F00F
Overflow; histogram overflow
00F0
0010
F010
No access
00F0
0011
F011
Data type requested does not match data available
00F0
0012
F012
Incorrect command parameters
00F0
0013
F013
Address reference exists to deleted area
00F0
0014
F014
Command execution failure for unknown reason
PLC-3® histogram overflow
00F0
0015
F015
Data conversion error
00F0
0016
F016
The scanner is not available to communicate with a 1771 rack adapter
00F0
0017
F017
The adapter is no available to communicate with the module
00F0
0018
F018
The 1771 module response was not valid
00F0
0019
F019
Duplicate label
00F0
001A
F01A
File owner active - the file is being used
00F0
001B
F01B
Program owner active - someone is downloading or editing online
00F0
001C
F01C
Disk file is write protected or otherwise not accessible (offline only)
00F0
001D
F01D
Disk file is being used by another application
Update not performed (offline only)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal