Multicasting Input Data

I/O input data is multicast in a system allowing multiple controllers to receive the input data. Controllers can request the input data by establishing a controlling connection to an input module or by requesting a listen-only connection. In either instance, the module responds back with the ID on which it is broadcasting the information. This allows the controller to
tune in
to the broadcast data and thus use it for control.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal