Flash Update

The module is either ready to update or is currently updating its firmware via an electronic flash update. (The ControlFLASH software tool is probably performing the flash update.)
module
A device, typically an I/O device, that communicates with the controller. The controller, a particular 1756-IB16I or a PanelView are all considered modules.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal