Configure an isolated integer analog output module

Create a channel-level configuration specific to an application.
To configure an isolated integer analog output module:
  1. Select the channel button for the channel that you want to configure.
  2. Select the
    Hold for Init
    box if you want the module to hold the output signal unchanged until the output value (received from the controller) is within 0.1% of full scale of the value held.
  3. Select the
    Hold
    button (under Fault State) if you want the output channel to remain at the last output value, OR
  4. Select the down arrow (under Fault State) if you want the output channel to go to a specific value if the connection, to the owner controller, is lost.
    A User button appears. Select the
    User
    button.
    TIP:
    If you performed this step, please go to the next step. If you did not perform this step, please skip Step 5 and proceed with Step 6.
  5. Enter a value for the output to take upon fault in User Fault Value.
  6. Select the
    Ramp to Fault
    box for each output point for which you want to enable ramping, at the ramp rate limit, from the current output value to the fault value (when a fault occurs).
  7. Select the
    Hold
    button (under Program State) if you want the output channel to remain at the last output value, OR
  8. Select the down arrow (under Program State) if you want the output channel to go to a specific value if the owner controller is switched into program mode.
    A
    User
    button appears. Select the
    User
    button.
    TIP:
    If you performed this step, please go to the next step. If you did not perform this step, please skip Step 5 and proceed with Step 6.
  9. Enter a value for the output to take, when the module enters program state, in
    User Program Value
    .
  10. Select the
    Ramp to Program
    box for each output point that you want to enable ramping, at the current rate limit, from the current output value to the program value (when a program command is received from the controller).
  11. Enter the maximum rate of change in the output signal for each output point, in counts per second, in
    Rate Limit
    .
  12. Select
    OK
    to save the changes to close the dialog.
    TIP:
    For information about what to do when a communication failure occurs, please refer to the Overview topic listed under See also below.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal