Configure a non-isolated analog output module- floating point

Create a channel-level configuration specific to your application.
To configure a non-isolated analog output module (floating point):
    1. In the
      Controller Organizer
      , right-click the module and select
      Properties
      .
    2. In the
      Module Propertie
      s dialog, select the
      Configuration
      tab.
    3. Select the
      Channel
      button to select the channel to configure.
    Enter the appropriate
    Scaling
    values for:
    • Low Signal
    • Low Engineering
    • High Signal
    • High Engineering
  1. In the
    Output Range
    box, select the output range of the module.
  2. In the
    Sensor Offset
    box, enter a value to compensate for sensor inaccuracies during calibration.
  3. Select
    Hold for Initialization
    to have the module hold the output signal unchanged until the output value (received from the controller) is within 0.1% of full scale of the value held.
    1. Select
      Apply
      to save the changes and continue editing, or select
      OK
      to save the changes and close the dialog.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal