Calibration Wizard - Select Channels to Calibrate Tab 1756 Analog I/O

This tab allows you to select the channel(s) you want to calibrate using the
Calibrate?
check box.
You can calibrate any combination of channels in groups or calibrate all channels at once by selecting the
Calibrate Channels in Groups
or
Calibrate Channels One at a Time
radio buttons. We recommend you calibrate all the channels on your module each time. This helps you maintain consistent calibration readings and improve module accuracy.
module
A device, typically an I/O device, that communicates with the controller. The controller, a particular 1756-IB16I or a PanelView are all considered modules.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal